Part Number: EVM430-FR6047
Other Parts Discussed in Thread: UNIFLASH
Hi,
I use the EVM430-FR6047 connenct to the PC, but it shows there are two port connected(show below), the location info is the same. I have trasfer to another PC, still two ports.
In this situaiton, I use the UNIFLASH and CCS, it work normal, can download the codes, but when I connect to the USS, it can't be connected and show the notice(see below).
Another info is I have put the EVM430-FR6047 connected to the USB Docking station. Before that, I was connect the PC directly and the USS was working well.
Now, what should I do?