This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5418A利用TimeB控制ADC多通道频率采用问题



程序目的是以2000Hz频率采样思路数据,ADC采用序列通道模式,TimeB.OUT1控制。由TimeB.OUT1的频率决定ADC采样频率。现在问题是程序只响应一次中断,不知道哪儿有问题,请专家指点。

程序主要部分如下:

* XT2晶振 20MHZ

* MCLK = 20MHz,

* SMCLK =20MHZ

* ACLK =0.625MHZ,

#include <msp430x54xA.h>

unsigned int results[4];    

//************************************************************#define SMCLK 20000000     //SMCLK频率

#define Hz 50     //频率

#define point 40  //采样点数

/*************************************************

 函数(模块)名称:void Init_TB(void)

 功能: 定时器B初始化

*************************************************/

void Init_TB(void)

{

 //\*************************************************************  //示波器观察

  P4DIR|= BIT1;     //方向选择      TB0 CCR1输出,示波器观察 0.5ms(500us)一个周期

  P4SEL|= BIT1;     //端口功能选择

 //\*************************************************************  //Setup Timer B0

 TBCCR0 = SMCLK/(Hz*point);

 TBCCR1 = TBCCR0/2;

 TBCCTL1 = OUTMOD_3;                       // CCR1 set/reset mode

 TBCTL = TBSSEL_2+MC_1+TBCLR;              // SMCLK, Up-Mode,Timer_B clear.

 //TBCTL = TBSSEL_2+MC_1;  

}

/*************************************************

 函数(模块)名称:void Init_ADC12(void)

 功能: ADC12初始化

*************************************************/

void Init_ADC12(void)

{

 P6SEL = 0x0F;                             // Enable A/D channel inputs

/* Initialize ADC12_A */

 ADC12CTL0 = ADC12ON+ADC12MSC+ADC12SHT0_2; // Turn on ADC12, set sampling time

 ADC12CTL1 = ADC12CSTARTADD_0+ADC12SHS_3+ADC12SHP+ADC12DIV_3+ADC12SSEL_2+ADC12CONSEQ_1;      

 ADC12CTL2=ADC12TCOFF+ADC12RES_2;

 ADC12MCTL0 = ADC12INCH_0;                

 ADC12MCTL1 = ADC12INCH_1;                

 ADC12MCTL2 = ADC12INCH_2;                

 ADC12MCTL3 = ADC12INCH_3+ADC12EOS;        

 ADC12IE = 0x08;                           // Enable ADC12IFG.3

 ADC12CTL0 |= ADC12ENC;                    // Enable conversions

}

void main(void)

{    

     WDTCTL = WDTPW + WDTHOLD;                       // 停止看门狗

     P1DIR|= BIT4;     //示波器观察窗口

     Init_Clk();//时钟初始化

     Init_ADC12();//ADC12初始化

     Init_TB();//TB初始化

      __enable_interrupt();

     for(;;)

     {

       _NOP();

     }

}

#pragma vector=ADC12_VECTOR

__interrupt void ADC12ISR (void)

{

 switch(__even_in_range(ADC12IV,34))

 {

 case  0: break;                           // Vector  0:  No interrupt

 case  2: break;                           // Vector  2:  ADC overflow

 case  4: break;                           // Vector  4:  ADC timing overflow

 case  6: break;                           // Vector  6:  ADC12IFG0

 case  8: break;                           // Vector  8:  ADC12IFG1

 case 10: break;                           // Vector 10:  ADC12IFG2

 case 12:                                  // Vector 12:  ADC12IFG3

   _NOP();

   results[0] = ADC12MEM0;                 // Move results, IFG is cleared

   results[1] = ADC12MEM1;                 // Move results, IFG is cleared

   results[2] = ADC12MEM2;                 // Move results, IFG is cleared

   results[3] = ADC12MEM3;                 // Move results, IFG is cleared

   P1OUT ^= BIT4;

   break;

 case 14: break;                           // Vector 14:  ADC12IFG4

 case 16: break;                           // Vector 16:  ADC12IFG5

 case 18: break;                           // Vector 18:  ADC12IFG6

 case 20: break;                           // Vector 20:  ADC12IFG7

 case 22: break;                           // Vector 22:  ADC12IFG8

 case 24: break;                           // Vector 24:  ADC12IFG9

 case 26: break;                           // Vector 26:  ADC12IFG10

 case 28: break;                           // Vector 28:  ADC12IFG11

 case 30: break;                           // Vector 30:  ADC12IFG12

 case 32: break;                           // Vector 32:  ADC12IFG13

 case 34: break;                           // Vector 34:  ADC12IFG14

 default: break;

 }

}