This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430 8M晶振问题



以下程序是实验msp430单片机在8M下使P2.0口输出方波。但是烧进单片机里发现P2.0口频率很低(可以看见led在那里闪)。照理P2.0口输出频率很高才对啊 
 50000/8M=0.00625 秒才对啊  还有改为  BCSCTL2|=SELM_2+DIVM_3;   改后根本没有分频啊;        求高手帮我分析下为什么啊。

#include  <msp430x14x.h>
void main(void)
{
  unsigned int i;
  WDTCTL=WDTPW+WDTHOLD;      //停止看门狗
  P2DIR|=0xFF;               //P5.4输出
  P2OUT|=0xFF;               //P5.4用作MCLK输出
  BCSCTL1&=~XT2OFF;          //XT2有效
  do
  {
    IFG1&=~OFIFG;             //清除振荡器失效标志
    for(i=0xFF;i>0;i--);     //稳定时间
  }
  while((IFG1&OFIFG)!=0);    //如果振荡器失效标志存在
  BCSCTL2|=SELM_2;            //MCLK=XT2
  TACTL=TASSEL_2+TACLR;
  CCTL0=CCIE;
  CCR0=50000;
  
  TACTL|=MC0;
  _EINT();

  for(;;)
  {
 
  }
}

#pragma vector=TIMERA0_VECTOR
__interrupt void Timer_A (void)
{
  P2OUT^=0x01;
}