This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430中DCOSEL(3位)、DCO(5位)、MOD(5位)之间的关系?



DCOSEL(3位)是选择8个频率范围之一作为fDCO频率范围;DCO(5位)是对所选择的fDCO频率范围进行32个范围划分;MOD(5位)的作用是什么呢?是对32个频率之间进行切换么?(例如:若MOD(5位)=00010B,则表示在DCO(5位)所选定的fDCO频率范围和fDCO+1频率范围间进行插入2个周期数得到所要求的fDCO频率) 关于MOD作用比较迷糊,还得大家多多指点。

例外还有一处英文资料不明白其中的意思,请大家给予通俗易懂的指点:

The DCO register value is incremented when the modulation bit counter rolls over from 31 to 0. If the modulation bit counter decrements from 0 to the maximum count, the DCO register value is also decremented.