This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询一个430ADC的问题



假如采样频率是300Hz,用的是16位AD,采样的数据要保存在256K的FLASH芯片中,请问最多可以记录多长时间?

  • 你的flash是256kb,还是256kB?
  • 你好!

    假如采样频率是300Hz,每次采样多少个点?

    用的是16位AD,ADC转换取多少有效位?

    采样的数据要保存在256K的FLASH芯片中,明确一下是256K BIT还是256K BYTE?

    另外这个Flash中可用于数据存储的空间有多少?是否还有其他数据存储在这个上面?

    举个例子,如果是256K BYTE均可存储数据,转换结果是16bit的,每次采一个点,则可以记录的时间是:

    256*1024/2/300 = 436.9s