This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP432的内部温度传感器使用



最近刚拿到MSP432,在跑ADC14部分的程序时,发现内部温度传感器的程序有问题,数据一直为0。

我分别跑了2个例程,1个是寄存器操作的,另外1个是驱动库的,存在的问题一样:读取30度和85度的校正值有问题。

1.寄存器操作定义了:

#define CALADC_15V_30C *((unsigned int *)0x1A1A) // Temperature Sensor Calibration-30 C
// See device datasheet for TLV table memory mapping
#define CALADC_15V_85C *((unsigned int *)0x1A1C) // Temperature Sensor Calibration-85 C

我看不懂0x1A1A 和0x1A1C这个指针到底是指向哪里?datasheet也没有!

2.驱动库:

cal30=SysCtl_getTempCalibrationConstant(SYSCTL_2_5V_REF,SYSCTL_30_DEGREES_C);

cal85=SysCtl_getTempCalibrationConstant(SYSCTL_2_5V_REF,SYSCTL_85_DEGREES_C);

tempC=(float)(((uint32_t)ADC14_getResult(ADC_MEM0)-cal30)*(85-30))/(cal85-cal30)+30.0f;

我看了驱动库手册,SysCtl_getTempCalibrationConstant()的定义,它返回none,这里这样引用该函数,显然有问题!TI能否提供详细一点的datasheet!这2个校正值在TLV里,但我没有在datasheet找到。

Retrieves the calibration constant of the temperature sensor to be used
//! in temperature calculation.
//!
//! \param refVoltage Reference voltage being used.
//!
//! The \e resetType parameter must be only one of the following values:
//!         - \b SYSCTL_1_2V_REF
//!         - \b SYSCTL_1_45V_REF
//!         - \b SYSCTL_2_5V_REF
//!
//! \param temperature is the calibration temperature that the user wants to be
//!     returned.
//!
//! The \e temperature parameter must be only one of the following values:
//!         - \b SYSCTL_30_DEGREES_C
//!         - \b SYSCTL_85_DEGREES_C
//!
//! \return None.