This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6736串口通信程序的问题,求解答。

我利用官方给的程序进行串口通信,想在串口助手上输出一段字符串,可是串口助手没有反应,麻烦大家帮忙看看,谢谢啦。

这是代码:

#include <msp430.h>
#include <math.h>
unsigned char buffer[]={"I'm MSP430!\n"};
void delay(unsigned int n)
{

unsigned int i,j;

for(i=0;i<n;i++)
for(j=0;j<100;j++);
}
void main(void)
{
unsigned int i;
WDTCTL = WDTPW | WDTHOLD;               // Stop WDT
// Setup P2.4 UCA0RXD, P2.5 UCA0TXD
P2SEL |= BIT4 | BIT5;                                     // Set P2.4, P2.5 to non-IO
P2DIR |= BIT4 | BIT5;                                     // Enable UCA0RXD, UCA0TXD
//Setup LFXT1
UCSCTL6 &= ~(XT1OFF); // XT1 On
UCSCTL6 |= XCAP_3;                                 // Internal load cap
// Loop until XT1 fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG);

SFRIFG1 &= ~OFIFG; // Clear fault flags
} while (SFRIFG1 & OFIFG);                                     // Test oscillator fault flag
// Setup eUSCI_A0
UCA0CTLW0 |= UCSWRST;                                  // **Put state machine in reset**
UCA0CTLW0 |= UCSSEL_1;                                  // CLK = ACLK
UCA0BRW_L = 0x03;                                              // 32kHz/9600=3.41 (see User's Guide)
UCA0BRW_H = 0x00; 
UCA0MCTLW = 0x5300;                                    // Modulation UCBRSx=0x53, UCBRFx=0
UCA0CTLW0 &= ~UCSWRST;                         // **Initialize USCI state machine**
UCA0IE |= UCTXIE;                                           // Enable USCI_A0 RX interrupt
while(1)
{
while (!(UCA0IFG & UCTXIFG)) ;                     // USCI_A0 TX buffer ready?
for(i=0;i<sizeof(buffer);i++)
{
UCA0TXBUF=buffer[i];
delay(20);
}
}
}

  • 什么开发板?哪个程序?

  • 你好,我是买来芯片自己做的一块板子,参考程序:

    #include <msp430.h>

    void main(void)
    {
    WDTCTL = WDTPW | WDTHOLD; // Stop WDT

    // Setup P1.2 UCA0RXD, P1.3 UCA0TXD
    P1SEL |= BIT2 | BIT3; // Set P1.2, P1.3 to non-IO
    P1DIR |= BIT2 | BIT3; // Enable UCA0RXD, UCA0TXD

    // Setup LFXT1
    UCSCTL6 &= ~(XT1OFF); // XT1 On
    UCSCTL6 |= XCAP_3; // Internal load cap
    // Loop until XT1 fault flag is cleared
    do
    {
    UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG);
    // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG;                                                      // Clear fault flags
    } while (SFRIFG1 & OFIFG);                                          // Test oscillator fault flag

    // Setup eUSCI_A0
    UCA0CTLW0 |= UCSWRST;                                       // **Put state machine in reset**
    UCA0CTLW0 |= UCSSEL_1;                                      // CLK = ACLK
    UCA0BRW_L = 0x03;                                                   // 32kHz/9600=3.41 (see User's Guide)
    UCA0BRW_H = 0x00; //
    UCA0MCTLW = 0x5300;                                          // Modulation UCBRSx=0x53, UCBRFx=0
    UCA0CTLW0 &= ~UCSWRST;                                   // **Initialize USCI state machine**
    UCA0IE |= UCRXIE;                                                    // Enable USCI_A0 RX interrupt

    __bis_SR_register(LPM3_bits | GIE);                    // Enter LPM3, interrupts enabled
    __no_operation();                                                       // For debugger
    }

    // USCI_A0 interrupt service routine
    #pragma vector=USCI_A0_VECTOR
    __interrupt void USCI_A0_ISR(void)
    {
    switch (__even_in_range(UCA0IV, 4))
    {
    case USCI_NONE: break;                                      // No interrupt
    case USCI_UART_UCRXIFG:                               // RXIFG
    while (!(UCA0IFG & UCTXIFG)) ;                           // USCI_A0 TX buffer ready?
    UCA0TXBUF = UCA0RXBUF;                                // TX -> RXed character
    break;
    case USCI_UART_UCTXIFG: break;                 // TXIFG
    case USCI_UART_UCSTTIFG: break;             // TTIFG
    case USCI_UART_UCTXCPTIFG: break;            // TXCPTIFG
    default: break;
    }
    }

  • 您好,我是自己买来芯片做的板子,参考程序:

    #include <msp430.h>

    void main(void)
    {
    WDTCTL = WDTPW | WDTHOLD; // Stop WDT

    // Setup P1.2 UCA0RXD, P1.3 UCA0TXD
    P1SEL |= BIT2 | BIT3; // Set P1.2, P1.3 to non-IO
    P1DIR |= BIT2 | BIT3; // Enable UCA0RXD, UCA0TXD

    // Setup LFXT1
    UCSCTL6 &= ~(XT1OFF); // XT1 On
    UCSCTL6 |= XCAP_3; // Internal load cap
    // Loop until XT1 fault flag is cleared
    do
    {
    UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG);
    // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG; 
    } while (SFRIFG1 & OFIFG); 

    // Setup eUSCI_A0
    UCA0CTLW0 |= UCSWRST; 
    UCA0CTLW0 |= UCSSEL_1;                             // CLK = ACLK
    UCA0BRW_L = 0x03;                                          // 32kHz/9600=3.41 (see User's Guide)
    UCA0BRW_H = 0x00; //
    UCA0MCTLW = 0x5300;                                   // Modulation UCBRSx=0x53, UCBRFx=0
    UCA0CTLW0 &= ~UCSWRST;                            // **Initialize USCI state machine**
    UCA0IE |= UCRXIE;                                           // Enable USCI_A0 RX interrupt

    __bis_SR_register(LPM3_bits | GIE);             // Enter LPM3, interrupts enabled
    __no_operation();                                         // For debugger
    }

    // USCI_A0 interrupt service routine
    #pragma vector=USCI_A0_VECTOR
    __interrupt void USCI_A0_ISR(void)
    {
    switch (__even_in_range(UCA0IV, 4))
    {
    case USCI_NONE: break;                                    // No interrupt
    case USCI_UART_UCRXIFG:                           // RXIFG
    while (!(UCA0IFG & UCTXIFG)) ;                        // USCI_A0 TX buffer ready?
    UCA0TXBUF = UCA0RXBUF;                         // TX -> RXed character
    break;
    case USCI_UART_UCTXIFG: break;                // TXIFG
    case USCI_UART_UCSTTIFG: break;                // TTIFG
    case USCI_UART_UCTXCPTIFG: break;            // TXCPTIFG
    default: break;
    }
    }

  • 这个代码是echo的,是你用调试助手发,单片机收到了,再把收到的发出去在调试中断显示出来

    while (!(UCA0IFG & UCTXIFG)) ;                        // USCI_A0 TX buffer ready?
    UCA0TXBUF = UCA0RXBUF;                         // TX -> RXed character
    break;

    你看看是不是流程错了。

    如果操作对的话,尝试在

    case USCI_UART_UCTXIFG: break;                // TXIFG

    UCA0TXBUF = 0x55

    如果还不对,检查你的时钟,管脚配置对不对,是在不行换个调试助手试试

  • 谢谢您的耐心解答,我还是太业余了,先从基础看起吧。

  • 如果是自己做的板子,建议先把RX和TX短接,用单片机发送一个字符看能不能收到。如果能正确收到,说明板子在硬件上没有问题。

  • 您好,我将RX和TX短接后,向板子发送字符再返回时正常的,但和其他设备串口通信时返回值就会乱码,请问这是什么原因?谢谢了~

  • shari zhang 说:

    您好,我将RX和TX短接后,向板子���送字符再返回时正常的,但和其他设备串口通信时返回值就会乱码,请问这是什么原因?谢谢了~

    有可能是你两边配置的串口通讯格式不同

  • 您好,串口两边配置的串口通信格式具体指的是什么?波特率吗?有可能是板子上的XT1晶振有问题吗?