最近在学习MSP430F4152 INFO段的读写操作,但网上部分网友反映INFO段的A段不能擦出,A段保存单片机部分数据,擦除单片机会出问题,请问各位专家MSP430F4152单片机能否擦除A区???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在学习MSP430F4152 INFO段的读写操作,但网上部分网友反映INFO段的A段不能擦出,A段保存单片机部分数据,擦除单片机会出问题,请问各位专家MSP430F4152单片机能否擦除A区???
void write_SegA (char value)
{
int *Flash_ptr; // Flash pointer
unsigned char i;
Flash_ptr = (int *) 0x1080; // Initialize Flash pointer
FCTL1 = FWKEY + ERASE; // Set Erase bit
FCTL3 = FWKEY; // Clear Lock bit
*Flash_ptr = 0; // Dummy write to erase Flash segment
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
for (i=0; i<128; i++)
{
*Flash_ptr++ = value; // Write value to flash
}
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}
十分感谢您的帮助,我看到的A段里面都是FF,论坛之前有人说A段保存单片机参数,比如晶振校正参数之类的,想问您下,什么情况下才可以确定“完全可以进行擦除掉”。
强烈建议不要擦除,因为里面保存了DCO和内部温度传感器的校正值。
另外如果需要使用information bank的话,建议还是使用 B,C,D三个区。
谢谢