This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430中的SPI配置



SPI协议,多主多从怎么理解?多主多从那又是怎么配置的,还有SPI在低功耗下怎么配置比较好点?

  • 多主多从的SPI我不是太了解.

    关于SPI的低功耗,以USCI为例 分为主/从两种情况

    1.如果是从设备(slave): 由于clock是从外部获得,所以 slave 可以停掉内部所有的时钟,进入较深的低功耗模式,比如LPM4。 数据发送和接收都能产生中断唤醒MCU

    2.如果是主设备(Master),SPI的时钟是自动使能和关闭的。

    简而言之,MSP430的SPI足够智能化来保持最低功耗,不需特别的配置。