#include <msp430.h>
void main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
// to activate previously configured port settings
P1DIR = 0x01; // Set P1.0 to output direction
P1OUT = 0x00;
P1REN = 0x00;
while(1){
if ((P1IN & 0x08) == 0x08)
P1OUT = 0x01;
else
P1OUT = 0x00;
}
}
In this code, i am try to achieve a voltage detecttion, however, i don't know the meaning of code "PM5CTL0 &= ~LOCKLPM5;". if i delete it, the output of specific pin would keep in off state.
So i want to the accurate meaning of the code "PM5CTL0 &= ~LOCKLPM5;" and how to use it correctly.