MSP430FR6043: 移植MSP430FR6043的Gas_Demo遇见障碍,需要帮助与引导

Part Number: MSP430FR6043

移植MSP430FR6043的FR6043_USSSWLib_template_example与MSP430FR6043EVM_USS_Gas_Demo工程中,报错
Description Resource Path Location Type
#16019-D file "../lib/IQMathLibrary/libraries/CCS/MPY32/5xx_6xx/IQmathLib_CCS_MPY32_5xx_6xx_CPUX_large_code_large_data.lib<__IQNmpy.o>" specifies large data memory model, which is not compatible with restricted large data memory model specified in a previous file or on the command line FR6043_USS_OAKO_Development C/C++ Problem
请问一下,想要移植MSP430FR6043的工程文件的时候,对于上述报错及其.a文件的移植处理是怎么样的?或者说,怎么样的步骤才算是正确的移植流程?