TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430—EXP5529编程错误问题‘error #10010: errors encountered during linking; "PWMout.out" not built’

Other Parts Discussed in Thread: MSP430F5529

/*
* main.c
*/
#include <msp430f5529.h>
void TAPwmSetPeriod (unsigned int Period);
void TAPwmSetDuty(unsigned int Duty);
void main(void)
{
WDTCTL = WDTPW + WDTHOLD;
P2DIR |= BIT0;
P2SEL |= BIT0;
//TA1CCTL2 = OUTMOD_7;
TA1CCTL1 = OUTMOD_7;
TA1CTL = TASSEL_1 + MC_1 + TACLR;
TAPwmSetPeriod (500); //通道1/2的PWM 方波周期均设为500个时钟周期
TAPwmSetDuty (200); //D[1]中的值作为占空比输出
__bis_SR_register(LPM3_bits); // Enter LPM3
__no_operation(); // For debugger
}

//增计数模式确定输的PWM周期
voidTAPwmSetPeriod (unsigned int Period)
{
TA1CCR0 = Period;
}
//占空比函数
voidTAPwmSetDuty(unsigned int Duty)
{

TA1CCR1=Duty;
}

程序如上,总有错误‘error #10010: errors encountered during linking; "PWMout.out" not built’

我是新手,怎么解决这个错误呢