This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP430F2618的时钟配置问题以及低功耗问题



我在我的硬件电路上只保留MCU和32K 晶振,将MCU设为LMP3模式,两种不同的时钟配置,得出不同的功耗,为什么会出现这种情况呢?

1、参考MSPWARE的LPM3例程,不对时钟进行配置,时钟ACLK = LFXT1/4 = 32768/4, MCLK = SMCLK = default DCO ~1.045MHz。

     BCSCTL1 |= DIVA_2;                        // ACLK/4 = 8.192 kHz

   测出40uA。

2、使用以下时钟函数,测出的功耗有1.35mA, 该时钟配置有什么问题没,为什么会对功耗影响这么大。

void cpu_init(void)
{
uint16 i;

asm(" BIS.W #40h,SR"); // disable DOC

/*select XT2*/
BCSCTL1 &= ~XT2OFF;

BCSCTL1 &= ~XTS;     // LFXT1 in LF MODE

BCSCTL1 &= ~0x30;    // ACLK,1分频,32768HZ。


/*SELM_2--选择XT2 for MCLK if XT2 Present,SELS--Select XT2 for SMCLK*/
BCSCTL2 |=(SELM_2+SELS);

/*SMCLK 8/4=2MHZ*/
BCSCTL2 |= (DIVS1); // SMCLK 4分频
BCSCTL3 |= XT2S_2; // Mode 2 for XT2 : 3- 16 MHz crstal

/*清除晶震错误标志*/
while (IFG1&OFIFG) {
      IFG1 &= 0x1;
BCSCTL3 &= 0xfc;
    /*等待清除完成*/
   for (i=0xff;i>0;i--)
     { }
   }
}