芯片是6733,用XT1的32768外设晶体,设主频25M,仿真状态下运行,发现XT1LFOFFG = 0,但DCOFFG和OFIFG都 = 1,感觉很奇怪,为什么XT1错误标志没有反应,但DCO错误置位了,而且在时钟中断里,看下来也是已经在25M下运行没有错。不用XT1,用REFOCLK就没有这个问题
还有个奇怪的现象是如果我在启动晶振的程序while (SFRIFG1&OFIFG) // Test oscillator fault flag 处设断点,程序就进入死循环,因为测到OFIFG = 1了,但如果一开始不设断点,直接运行,OFIFG 还是= 1,但会跑进主程序正常运行,这是仿真器的问题吗?
另外问一下各位高手,6733能不能接XT2?还是只能接XT1?(芯片引脚只有XIN,XOUT,没有XT2IN和XT2OUT),如果只能接XT1,能不能直接上25M的晶体?因为我看到XT1 有High-frequency 模式,XT1DRIVE设为11b时的描述是 Maximum drive capability and maximum current consumption for XT1 LF mode. XT1 oscillator operating range in HF mode is 24 MHz to 32 MHz.
下附晶振初始化的代码,请看看问题出在哪里?谢谢!
void setup_FLL(void) {//启动晶振和时钟; // Open PMM registers for write PMMCTL0_H = PMMPW_H; // Set VCore to new level PMMCTL0_L |= PMMCOREV_3; // Wait till new level reached if ((PMMIFG & SVMLIFG)) while ((PMMIFG & SVMLVLRIFG) == 0); // Lock PMM registers for write access PMMCTL0_H = 0x00; //用TX1做FLLREFCLK,主频选DCO // Initialize DCO to 25MHz UCSCTL6 &= ~(XT1OFF); // XT1 On do { UCSCTL7 &= ~XT1LFOFFG; // Clear XT1 fault flags } while (UCSCTL7 & XT1LFOFFG); // Test XT1 fault flag __bis_SR_register(SCG0); // Disable the FLL control loop UCSCTL3 = SELREF__XT1CLK; // Set DCO FLL reference = TX1 UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx UCSCTL1 = DCORSEL_7; // Select DCO range 50MHz operation UCSCTL2 = FLLD_0 | 762; // Set DCO Multiplier for 25MHz // (N + 1) * FLLRef = Fdco // (762 + 1) * 32768 = 25MHz // Set FLL Div(DCOCLKDIV) = fDCOCLK __bic_SR_register(SCG0); // Enable the FLL control loop // Worst-case settling time for the DCO when the DCO range bits have been // changed is n x 32 x 32 x f_MCLK / f_FLL_reference.. See UCS chapter in 5xx // UG for optimization. // 32 x 32 x 25 MHz / 32,768 Hz = 781250 = MCLK cycles for DCO to settle __delay_cycles(781250); while (SFRIFG1&OFIFG) // Test oscillator fault flag { UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG); // Clear XT2,XT1,DCO fault flags SFRIFG1 &= ~OFIFG; // Clear fault flags } UCSCTL4 |= SELA__XT1CLK+SELS__DCOCLKDIV + SELM__DCOCLK;//ACLK = XT1CLK;SMCLK = DCOCLKDIV;MCLK = DCOCLK }