msp430g2553有两个Timer A 每个有3个捕获比较模块,我数了一下TA0.0 有P1.1和P1.5,TA0.1有P1.2,P1.6,P2.6,没有看到有TA0.2;TA1.0有P2.0,P2.3;TA1.1有P2.1,P2.2;TA1.2有P2.4和P2.5;关于捕捉模式下这些端口都能用么,在PWM模式下为什么书上说最多只能产生3路PWM,这里这么多的端口为什么只有三路啊,由OUTMODX设置好输出模式后CCR1和R2都输出同种模式的PWM么,能不能只让某个IO输出PWM啊,谁能帮帮我理一理,书看的晕了,思路很混乱。