This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

#10010 errors encountered during linking; "MSP-EXP430F5529LP User Experiece20141117.out" not built

Other Parts Discussed in Thread: MSP-EXP430F5529LP, MSP430F5529

你好,我用得是MSP430F5529LP, 用CCS6.0编程,在导入程序后   编译时出现如下错误:

#10010 errors encountered during linking; "MSP-EXP430F5529LP User Experiece20141117.out" not built 

#10269 output file "MSP-EXP430F5529LP User Experiece20141117.out" exceeds code size limit 

**** Build of configuration Debug for project MSP-EXP430F5529LP User Experiece20141117 ****

"c:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building target: MSP-EXP430F5529LP User Experiece20141117.out'
'Invoking: MSP430 Linker'
"c:/ti/ccsv6/tools/compiler/msp430_4.3.3/bin/cl430" -vmspx --abi=eabi --data_model=restricted -O2 --advice:power="all" -g --gcc --define=__MSP430F5529__ --define=__LARGE_DATA_MODEL__ --diag_warning=225 --display_error_number --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU23 --silicon_errata=CPU40 --large_memory_model --printf_support=minimal -z -m"MSP-EXP430F5529LP User Experiece20141117.map" --heap_size=1000 --stack_size=1000 --use_hw_mpy=F5 -i"c:/ti/ccsv6/ccs_base/msp430/include" -i"C:/ti/TivaWare_C_Series-2.1.0.12573" -i"c:/ti/ccsv6/tools/compiler/msp430_4.3.3/lib" -i"c:/ti/ccsv6/tools/compiler/msp430_4.3.3/include" -i"C:/ti/TivaWare_C_Series-2.1.0.12573/driverlib/ccs/Debug/driverlib.lib" -i"c:/ti/ccsv6/ccs_base/msp430/lib" -i"c:/ti/ccsv6/ccs_base/msp430/lib/5xx_6xx_FRxx" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="MSP-EXP430F5529LP User Experiece20141117_linkInfo.xml" --rom_model -o "MSP-EXP430F5529LP User Experiece20141117.out" "./main.obj" "./src/Demo_OS.obj" "./src/global.obj" "./src/HAL/ADXL345.obj" "./src/HAL/DAC.obj" "./src/HAL/HCI.obj" "./src/HAL/Interrupt.obj" "./src/HAL/UserGraphic.obj" "./src/HAL/softFIFO.obj" "./src/HAL/softFilter.obj" "./src/Demo/Acceleration.obj" "./src/Demo/BJT_Characteristic _Curve.obj" "./src/Demo/DC_Motor.obj" "./src/Demo/IrDA.obj" "./src/Demo/Miscellaneous.obj" "./src/Demo/Music_Display.obj" "./src/Demo/Record.obj" "./src/Demo/Step_Motor.obj" "./src/Demo/Ultrasonic.obj" "./src/Demo/Weight.obj" "./src/Demo/White_LED.obj" "./sdCard/HAL_SDCard.obj" "./sdCard/wavType.obj" "./sdCard/FatFs/option/syscall.obj" "./sdCard/FatFs/ff.obj" "./sdCard/FatFs/mmc.obj" "./driverlib/adc10_a.obj" "./driverlib/adc12_a.obj" "./driverlib/aes.obj" "./driverlib/bak_batt.obj" "./driverlib/comp_b.obj" "./driverlib/crc.obj" "./driverlib/dac12_a.obj" "./driverlib/dma.obj" "./driverlib/eusci_a_spi.obj" "./driverlib/eusci_a_uart.obj" "./driverlib/eusci_b_i2c.obj" "./driverlib/eusci_b_spi.obj" "./driverlib/eusci_i2c.obj" "./driverlib/eusci_spi.obj" "./driverlib/eusci_uart.obj" "./driverlib/flash.obj" "./driverlib/gpio.obj" "./driverlib/ldopwr.obj" "./driverlib/mpy32.obj" "./driverlib/pmap.obj" "./driverlib/pmm.obj" "./driverlib/ram.obj" "./driverlib/ref.obj" "./driverlib/rtc_a.obj" "./driverlib/rtc_b.obj" "./driverlib/rtc_c.obj" "./driverlib/sd24_b.obj" "./driverlib/sfr.obj" "./driverlib/sys.obj" "./driverlib/tec.obj" "./driverlib/timer_a.obj" "./driverlib/timer_b.obj" "./driverlib/timer_d.obj" "./driverlib/tlv.obj" "./driverlib/ucs.obj" "./driverlib/usci_a_spi.obj" "./driverlib/usci_a_uart.obj" "./driverlib/usci_b_i2c.obj" "./driverlib/usci_b_spi.obj" "./driverlib/usci_i2c.obj" "./driverlib/usci_spi.obj" "./driverlib/usci_uart.obj" "./driverlib/wdt_a.obj" "./GRAPH/grlib/circle.obj" "./GRAPH/grlib/context.obj" "./GRAPH/grlib/image.obj" "./GRAPH/grlib/line.obj" "./GRAPH/grlib/rectangle.obj" "./GRAPH/grlib/string.obj" "./GRAPH/graphdriver/Template_Driver.obj" "./GRAPH/fonts/fontcm16b.obj" "./GRAPH/fonts/fontcm28b.obj" "./GRAPH/fonts/fontfixed6x8.obj" "./F5xx_F6xx_Core_Lib/HAL_FLASH.obj" "./F5xx_F6xx_Core_Lib/HAL_PMAP.obj" "./F5xx_F6xx_Core_Lib/HAL_PMM.obj" "./F5xx_F6xx_Core_Lib/HAL_TLV.obj" "./F5xx_F6xx_Core_Lib/HAL_UCS.obj" "./CTS/CTS_HAL.obj" "./CTS/CTS_Layer.obj" "./CTS/structure.obj" "../lnk_msp430f5529.cmd" -l"libc.a" -l"libmath.a"
<Linking>
remark #10372-D: (ULP 4.1) Detected uninitialized Port C in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.

error #10269: output file "MSP-EXP430F5529LP User Experiece20141117.out" exceeds code size limit
remark #10372-D: (ULP 4.1) Detected uninitialized Port D in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
error #10010: errors encountered during linking; "MSP-EXP430F5529LP User Experiece20141117.out" not built

>> Compilation failure
gmake: *** [MSP-EXP430F5529LP User Experiece20141117.out] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****

这个该怎么解决啊   求助。

x 出现错误。请重试或与管理员联系。