This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.



CC1100在TI的官网上有详细的天线设计链接为:www.ti.com.cn/.../cc1100em_pcb_ref_des
433MHz设计文档:www.ti.com.cn/.../cc1100em433_refdes 个人感觉TI的技术支持还是比较好的,很值得信赖。
我用的模块为利尔达的CC1100的模块,很好用的。
CC1100/1101/1150系列针对1GHz以下的应用;
CC2500系列针对2.5GHz的应用,不过这方面的我没用到,但是据说CC2500更便宜。
TI 关于这个开发板还有触摸板应用的视频从哪儿找啊?怎么一圈没找到,主要是触摸板的
提个小建议,MSP430的应用,尽量不要使用死循环,有机会就休眠,基本不会对系统性能造成影响,反而可以降低功耗。