Other Parts Discussed in Thread: ENERGIA
msp432p401r launchpad接到电脑上没有反应,但是之前接上去会提示安装驱动,可能是之前驱动安装过程错误导致,这种情况该怎么做,请教一下TI的老师们
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ENERGIA
msp432p401r launchpad接到电脑上没有反应,但是之前接上去会提示安装驱动,可能是之前驱动安装过程错误导致,这种情况该怎么做,请教一下TI的老师们
一般来说,安装了CCS之后,驱动是自动安装的。您也可以采用如下步骤
参考 http://energia.nu/guide/guide_windows/
void main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
PJSEL0 |= BIT2 | BIT3; // Configure PJ.2/3 for HFXT function
PJSEL1 &= ~(BIT2 | BIT3);
CSKEY = CSKEY_VAL; // Unlock CS module for register access
CSCTL2 |= HFXT_EN | HFXTFREQ_6 | HFXTDRIVE;
while(CSIFG & HFXTIFG)
CSCLRIFG |= CLR_HFXTIFG;
/* Select MCLK & HSMCLK = HFXT, no divider */
CSCTL1 = CSCTL1 & ~(SELM_M | DIVM_M | SELS_M | DIVHS_M) | SELM__HFXTCLK | SELS__HFXTCLK;
CSKEY = 0; // Lock CS module from unintended accesses
P1DIR |= BIT0;
P1OUT |= BIT0;
while(1)
{
P1OUT ^= BIT0;
}
}
P4.3引脚输出是48MHz,但是P1.0的LED的灯引脚点评切换的频率只有1M,为什么?按道理P1.0的切换频率也应该是48MHz的,请大神指教。现在等在回复