msp430f4152的P1口是否具有中断功能
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
一般我们不这么用,如果要测电阻或电容变化。可以用一个GPIO给电阻电容充放电,然后将锯齿波通过COMP转成方波,用timer去检测这个波形的周期,来检测电阻或电容。当然了,用ADC检测也是可以的。
因为对功耗要求比较高,所以不想用CA和定时器。在网上看到很多资料都是cmos端口能够这样实现的,我不知道cmos端口能否这样用?还想问一下我用IO口监测,是不是只有电平稳定了,端口才会检测到电平?4152哪几个是cmos端口?
可以啊,但这种方法一般demo起来没什么问题,但是量产一致性会比较差,因为I/O的阈值电压范围会比较宽泛点。一般到了从低到高的阈值,就会触发翻转,不一定要等充满。
我现在用这宫方法却不行,用P1口检测电压 的,但是IO口检测不到电容一端的电压?可以留个QQ吗?我们可以交流更快些