您好:
请问MSP430F5310的IO口在Full Drive Strength设置下,最大驱动电流能达到多少。我现在想用IO口输出高电平驱动6mA的负载,能否直接用IO口驱动,对IO口是否有损坏。我看数据手册上说,在VCC=3V工作条件下,I(OHmax) = –5 mA;I(OHmax) = –15 mA;是否最大驱动电流能达到15mA。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
请问MSP430F5310的IO口在Full Drive Strength设置下,最大驱动电流能达到多少。我现在想用IO口输出高电平驱动6mA的负载,能否直接用IO口驱动,对IO口是否有损坏。我看数据手册上说,在VCC=3V工作条件下,I(OHmax) = –5 mA;I(OHmax) = –15 mA;是否最大驱动电流能达到15mA。