This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430G2553测电源电压



我通过查看手册发现G2553内部有一个分压电阻可以读电源电压,通道为11,但是我读出的数据转换后得到的电压值明显低于电源电压,我使用的是lanunchpad板电压应为3.59V左右,测的的电压只有3.45V,后来使用分压电阻供电测量VCC发现读数一直不变,并不随电压变化而变化,有没有读电源电压的样例给我参考一下,谢谢大家帮忙

还有一个问题,如何才能提高AD的精度,AD10肯定不能变了,是不是可以通过调整采样时间或者类似参数提高精度,给个样例参考一下。谢谢