This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5234: 关于HOST使用I2C与MSP430进行主机接口协议通信

Part Number: MSP430F5234
Other Parts Discussed in Thread: TIDA-050026-23881, TPS23881

参考TPS2388x PSE System Firmware Host Interface Protocol文档

  • 使用HOST与MSP430进行I2C通信,使用i2ctransfer命令工具按照主机协议发送对应数据格式
  • 在发送关于带有Password (0xC430)的数据,功能似乎没有生效,需要如何验证?
  • 在执行I2ctransfer指令发送对应的数据包之后观察使用的是POE EVB(TIDA-050026-23881)
  • 后续我应该如何编写i2c代码在我的host中去控制MSP430从而间接控制PSE系统?
  • 是否我只需要关注HOST与MSP430之间的通信过程即可,而不需要关心MCU:MSP430与PSE:TPS23881之间的具体通信?(MSP中烧写了关于POE的固件系统)

以下是其中两个相关:

1.使用I2ctransfer指令:i2ctransfer -f -y 0 w5@0x48 0x01 0x02 0xC4 0x30 0xF7

 

2.使用I2ctransfer指令:i2ctransfer -f -y 0 w5@0x48 0x03 0x02 0xC4 0x30 0xF5

如果你了解这些,期待你的回复,十分感谢!