Part Number: LP-MSPM0G3507
依照提示update之后出现报错内容:
CS_DAP_0: Error initializing emulator: (Error -591 @ 0x0) The firmware updater encountered an error and could not finish. The updater failed to connect to the XDS110 in programming mode. Unplug and re-plug the XDS110, and try again. If the problem remains, try updating the firmware using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of the installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 12.8.0.00194)