This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F149复位时碰到奇怪的问题。



在给系统供电反复快速下电的时候会很容易出现430无法正常启动的情况,出现这种情况后再断电(短时间)重新上电都会一直这样;

使用10K+0.1U的RC时碰到的,使用47K+0.1U可以解决;

感觉一定是复位的问题,但没办法合理解释;

149的spec里面标注的RST的VIL电压是VSS~VSS+0.6V,但是实测异常情况发生时,即使RST电压掉到0.6V以下还是不会正常复位,感觉很困惑。