This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430F2272在使用电池供电时,CPU会出现重启

Other Parts Discussed in Thread: CC1120

使用3V纽扣电池供电。430F2272和CC1120一起工作,CPU会定时通过CC1120发射数据。

在测试会出现CPU经常复位,一开怀疑是复位管脚电压跌落引起的复位。通过测量电压最低大概在2.4V左右。因此排除了。

最后怀疑是由于BOR电压跌落引起的,通过测量电压最低为2.3V左右。也是低于手册里面的1.71V。

现在就不知道该如何处理了,有人遇到过类似问题没有。

有什么办法可以避免这种问题。

先谢谢了