This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2618烧录进FLASH里的程序上电后不运行



如题,我将程序用IAR和FET-PRO430-LITE两种方式烧录到FLASH 中,通过VIEW看了FLASH中的数据,并比对了.TXT的程序问题,从0x3100位置开始,0xfffe和0xffff位置也是3100地址,并且通过IAR的debug仿真能够运行。但是片子单独上电后,却不运行,一个所有管脚都拉高的程序没反应,串口传输的也没没反应,管脚输出SMCLK也不行,同样程序烧录到后来买的开发板上就可以运行,并且别对了两个F2618的FLASH内存数据,也是一样,求大神指导,让单片机自己在上电后运行FLASH里的程序 谢谢