Part Number: MSP430F5438A
Other Parts Discussed in Thread: OPA2333,
求助,最近在用MSP430F5438A的ADC功能,采用ADI的LTC6115进行电流采集,信号经过ADI的模拟开关ADG708BRUZ以及TI的运算放大器OPA2333后输入给MSP430。信号电压范围设计的是0~5V,OPA2333做了个二分之一,给到MSP430信号电压是0~2.5V。如下图,绿色和黄色分别为ADG708输入前通道2和通道4的信号,红色为ADG708输出信号,可以看到当选通当前通道后,信号电压即刻被下拉下来,且在不同电压输入信号情况下的下拉幅度不一致,如图2图3。



下图蓝色为经过OPA2333后的信号,可以看到与ADG708输出信号相比刚好为其二分之一。

下图为相关芯片相关参数。



我的电路中,从LTC6115信号输出到ADG708信号输入中间的电缆长度大约有4到5米,不知道电压被下来是否是电缆造成的?或者是MSP430配置上的问题?