This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 LaunchPad设计心得】+模数中的魔术

Other Parts Discussed in Thread: MSP430G2231

数据可以通过查看寄存器得到!

#include <msp430g2231.h>  

volatile long tempRaw;存放ADC转换数值的
void main(void)
{
  volatile unsigned int i;                  
   
  WDTCTL = WDTPW + WDTHOLD;               停用看门狗  
if (CALBC1_1MHZ ==0xFF || CALDCO_1MHZ == 0xFF)                     
    while(1);                 启动ADO为MCLK
BCSCTL1 = CALBC1_1MHZ;   
  DCOCTL = CALDCO_1MHZ;         
   
  BCSCTL3 |= LFXT1S_2;                    
  IFG1 &= ~OFIFG;                        
  BCSCTL2 |= SELM_0 + DIVM_3;            使用DCO八分频
  
  while(1)
  {
   ADC10CTL1 = INCH_10 + ADC10DIV_0;      选择通道
   ADC10CTL0 = SREF_1 + ADC10SHT_3 + REFON + ADC10ON; 开启REF和ADC10
   _delay_cycles(5);                      等待参考设置
   ADC10CTL0 |= ENC + ADC10SC;             启动转换
      _delay_cycles(100);      等待转换
   ADC10CTL0 &= ~ENC;      停止ADc转换
   ADC10CTL0 &= ~(REFON + ADC10ON);        
   tempRaw = ADC10MEM;    、
   _delay_cycles(125000);      
  }
}