msp430的低频时钟选择为2.4mhz,然后再将其分频到300k,能否实现。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你这的低频时钟应该指的是LFXT1CLK吧。如果是这个的话,你将它选为2.4MHz,其实是用了LFXT1CLK的HF Mode。此时,首先需要注意,你选用的器件是否支持LFXT1CLK的HF Mode。
例如:MSP430x20xx, MSP430G2xxx的LFXT1是不支持HF Mode的,可用从对应Data Sheet中具体查看。
而例如:MSP430F2618则是支持HF Mode的,LFXT1Sx不同,则对应的频率也不同。下图从datasheet中截取

msp430f235的话,按照你的想法,你只需要在LFXT1外接一个2.4MHz的晶振,将其配置为HF Mode,并将其作为ACLK的clock源,8分频即可得到300KHz. msp430f235的DCO对应的16Mhz,出厂时是校准过的,你可以直接用它作为MCLK和SMLK的clock源。