This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5989的库函数开发时GPIO口输出问题



今天在用fr5989控制IO口时遇到了不知名问题,
是这样的,程序中没有时钟,所以使用的是默认的DCO,可是控制IO口输出电平时却没有任何现象;
代码如下:

#include "driverlib.h"

void main(void)
{
    //Stop WDT
    WDT_A_hold(WDT_A_BASE);


    GPIO_setAsOutputPin(GPIO_PORT_P1,GPIO_PIN2);

     GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN2);

     while(1)
     {
             GPIO_setOutputLowOnPin(GPIO_PORT_P1,GPIO_PIN2);
             for(uint8_t i=0;i<0xff;i++);
             GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN2);
             for(uint8_t i=0;i<0xff;i++);
     }
}

最后,把ACLK时钟引脚输出,用示波器也是还没发现有波形输出:

#include "driverlib.h"

void main(void)
{
    //Stop WDT
    WDT_A_hold(WDT_A_BASE);


    GPIO_setAsOutputPin(GPIO_PORT_P1,GPIO_PIN2);

     GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN2);
     GPIO_setAsOutputPin(GPIO_PORT_P5,GPIO_PIN2);
     GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P5,GPIO_PIN2,GPIO_SECONDARY_MODULE_FUNCTION);
     while(1)
     {
             GPIO_setOutputLowOnPin(GPIO_PORT_P1,GPIO_PIN2);
             for(uint8_t i=0;i<0xff;i++);
             GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN2);
             for(uint8_t i=0;i<0xff;i++);
     }
}

我新手,有谁看出问题所在吗。请教一下