This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f5529 launchpad 定时器A在比较输出两路pwm(模式4)时,两信号相位相对静止,但相位相对信号发生器发生变化,是怎么回事,谢谢解答



我还遇到了一个问题,我用定时器a的时候用比较输出模式4输出流两路PWM,这两路PWM的相位差确实是一定的,但是相对于信号发生器的相位却一直在改变,而我尝试用两台信号发生器对比的时候发现,两台信号发生器的pwm相位是相对静止的,现在我想要得到的是相对于信号发生器静止的信号,也就是说比较输出一旦确定输出流,那么相位就不要再变了,这该怎样处理

  • 因为msp430的PWM输出频率和你的信号发生器发出的信号频率是不同的。

    这种情况建议使用高精度的外部晶振作为时钟信号源,不要用dco。dco产生的频率本身都是在抖动,这是它的原理决定的。