大家好,我现在使用msp430F5510,只用了内部USB功能。我的问题是,在没有使用USB功能前,我的RAM用去1.7K左右,但是加上USB数据处理后,RAM超过了2K,但是这个芯片只有2KRAM,现在应该怎么办啊。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我现在使用msp430F5510,只用了内部USB功能。我的问题是,在没有使用USB功能前,我的RAM用去1.7K左右,但是加上USB数据处理后,RAM超过了2K,但是这个芯片只有2KRAM,现在应该怎么办啊。
55XX系列为USB功能分配了2K的RAM,当不使用USB时,这2K的RAM可以用作普通RAM。
5510内部有4k的通用RAM,和2K的USB RAM。总共有6K的ram