This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F149 使用bsl下载程序时出错

Other Parts Discussed in Thread: MSP430F149

使用MSP430FET下载程序的时候提示“Blank check failed. Protected function. Password not match“错误,无法下载。之前是可以下载的。在网上找了一些相关资料,说是MSP430坏了,需要换芯片。请问是这样吗?

  • 我简单看了一下《flash memory controller》那一章,关于password 05Ah这个应该是下载软件MSP430FET来负责处理的吧?用户使用该软件下载的时候不用关心?而且我之前是可以正常下载的,并且现在用同一型号的其他板子也是可以正常下载的。唯一只能怀疑是msp430坏掉了
    。不知道我分析的有道理吗?

  • 你用MSP430FET的仿真器还是什么?用工具能擦除整个flash么?擦除再写有问题么?

  • 用的MSPFET这个软件通过BSL下载,

    18:33:58 Device: MSP430F149. Info(0x1000-0x10FF), Main:(0x1100-0xFFFF)
    18:33:58 Erasing flash memory...
    18:34:00 Erase complete.
    18:34:00 Blank check device memory...
    18:34:01 Blank check failed. Protected function. Password not match.

    这是下载时报错日志。上次出现这个问题以后换了一个MSP430就好了,现在又有两片出现这个问题了。

  • 此贴终结。

    今天经过反复测试最后确定是由于下载时板子上给430提供的电源不干净,导致下载出错。与password无关,应该是下载软件误报。