我从msp430f6638的手册上看到USCI_B0 SPI模块的clock input/output和USCI_A0 的SPI slave transmit enable是共用同一根引脚,USCI_B1与USCI_A1也是如此。请问如果想同时使用USCI_B0和USCI_A0分别实现两路4线SPI通信,该如何实现?是否能利用其它通用输入输出接口作为SPI片选引脚?输入您的问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我从msp430f6638的手册上看到USCI_B0 SPI模块的clock input/output和USCI_A0 的SPI slave transmit enable是共用同一根引脚,USCI_B1与USCI_A1也是如此。请问如果想同时使用USCI_B0和USCI_A0分别实现两路4线SPI通信,该如何实现?是否能利用其它通用输入输出接口作为SPI片选引脚?输入您的问题
MSP4306638的P2管脚有PORT MAPPING的功能,简单来讲就是P2口可以映射成规定的数字IO口功能.
具体的操作就是设置P2管脚功能时,P2DIR =X, P2SEL.X = 1, P2MAPX= n
P2MAPX的值就是MAP的数字IO口功能索引。
按照楼主的需求,可以吧P2.0管脚映射到USBI_B0的STE上去。