• MSP-EXP430F5529LP: 请问 eZ-FET lite 需要到哪里去下载

    Part Number: MSP-EXP430F5529LP

    我看到手册中说到eZ-FET lite 是开源的,并且在User guide《MSP430F5529 LaunchPad Development Kit (MSP-EXP430F5529LP) User's Guide (Rev. D)》的2.2.2提供了一个网址:

    但是我点击这个网址显示的是404 not found

    请问是已经不再维护了么?我去哪里可以下载到这个固件?

  • MSP-EXP430F5529LP: 使用MSP-FET430UIF仿真器通过SBW的模式无法在线烧录仿真,错误报告是无法找到芯片。

    Part Number: MSP-EXP430F5529LP
    Other Parts Discussed in Thread: MSP430F5529

    在用MSP430F5529开发板的过程中,如果使用自带的USBmini接口可以仿真烧录程序,如果使用MSP-FET430UIF仿真器通过SBW的模式就无法下载仿真程序,故障显示是无法找到芯片。软件开发平台使用的是IAR V7.10 版本,电脑操作系统是WIN11。请问IAR的版本和WIN11的操作系统对仿真烧录有影响吗?为什么在SBW模式下无法仿真烧录…

  • MSP430F5529: 无法创建项目和烧板子

    Part Number: MSP430F5529

    一直创建不了项目,烧板子也一直显示灯准备中

  • MSP430F5529: XT2使用有源晶振时芯片不工作

    Part Number: MSP430F5529

    1.XT2使用外部4MHz的有源晶振时,只连接XT2IN,OUT悬空,晶振电源3.3V,MSP芯片无法工作,实测晶振已经起震,波形为方波,晶振输出串接22R电阻,15pF电容也不行

    2.XT2使用外部 晶振是否需要软件进行配置?对外部晶振的波形有无要求,如正弦波、方波

  • MSP430F5529: _disable_interrupts宏编译报警

    Part Number: MSP430F5529
    Other Parts Discussed in Thread: MSP430-SDK,

    Description Resource Path Location Type
    #48-D incompatible redefinition of macro "_disable_interrupts" (declared at line 129 of "D:/CCS11.0.0/ccs/tools/compiler/ti-cgt-msp430_21.6.0…

  • MSP430F5529: 通过MSP430的引脚P2.0发送PWM信号(3V的高低电平),从示波器观测到信号输出波形不正确,是一条横线?以下为测试连接图片和MSP430输出PWM信号代码,不知道哪里出了问题?

    Part Number: MSP430F5529

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    #include <msp430.h>
    #define TASSEL_SMCLK
    #define MC_UP
    int main(void)
    {
    WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
    //P2.0TA0.1(
    P2DIR |= BIT0;
    P2SEL |= BIT0;
    //SMCLK
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • MSP430F5529: 如何通过MSP430实现控制激光脉冲的发送?

    Part Number: MSP430F5529
    Other Parts Discussed in Thread: TDC7201

    目前通过MSP430与TDC7201连接实现对脉冲激光飞行时间的测量,脉冲激光器为外触发方式,如何通过MSP430实现控制激光脉冲的发送,具体需要MSP430的哪个引脚连接到激光器触发口?

  • MSP430F5529: 使用MSP430和TDC7201-ZAX-EVM结合进行激光测距,运行MSP430自带的例子程序会报如下错误:

    Part Number: MSP430F5529
    Other Parts Discussed in Thread: TDC7201-ZAX-EVM, , TDC7201

    使用MSP430和TDC7201-ZAX-EVM结合进行激光测距,运行MSP430自带的例子程序会报如下错误:

    gmake[1]: *** [tof.out] Error 2
    makefile:221: recipe for target 'tof.out' failed
    makefile:217: recipe for…

  • MSP430F5529: 我想知道如何去创建串口通信跟openmv进行数据交互,我找了一圈没有找到可以直接用的串口通信方案

    Part Number: MSP430F5529

    串口通信msp430f5529怎么跟openmv进行通信交互

  • MSP430F5529: 编译出错,不知道如何解决

    Part Number: MSP430F5529
    Other Parts Discussed in Thread: MSP-FET,

    Error initializing emulator:
    One of the connected MSP-FETs / eZ-FETs debuggers needs recovery. Select 'Recover' to start the recovery process.

    Note: Only one MSP-FET / eZ-FET debugger…

  • MSP430F5529: 新人求解,Error connecting to the target:Unknown device

    Part Number: MSP430F5529
    Other Parts Discussed in Thread: UNIFLASH

    新人求解,不清楚什么原因,无法烧录,也不能debug

  • MSP430F5529: PC的设备管理器无法识别MSP430

    Part Number: MSP430F5529

    电脑无法识别到开发板

  • MSP430F5529: 软件乱码问题

    Part Number: MSP430F5529

    软件注释乱码

  • MSP430F5529: fireware固件更新失败,无法修复

    Part Number: MSP430F5529
    Other Parts Discussed in Thread: MSP-FET

    我在第一次拿到这块msp430后就新建工作区尝试依据官方默认文件进行烧录,点烧录后提示升级固件,点击后发现固件更新失败。并出现如图画面。 Updating Fireware并没有任何进度。

    同时输出以下信息。

    MSP430: Error initializing emulator: One of the connected MSP-FETs / eZ-FETs debuggers…

  • MSP430F5529: Unable to burn program with CCS (MSP430F5529LP with type C port)

    Part Number: MSP430F5529

    Hi,

    I am trying to make my own MSP430F5529LP, and I change the type B port to type C port which is used to burning program.

    The following picture is the schematic diagram of the circuit.

    But it is unable to burn program with…

  • MSP430F5529: 在哪里可以取得io430.h和io430f5529.h文件?

    Part Number: MSP430F5529

    在网上下载了一个使用msp430f5529的关于RS485的MODBUS RTU协议的例程,例程里含有#include "io430.h"和#include "io430f5529.h"。运行程序,提示问题显示找不到这两个文件,CCS IDE版本是ccs 11.0.0。在msp430.h文件中也找不到该文件。

  • MSP430F5529: MSP430F5529的SPI屏蔽了按键中断问题

    Part Number: MSP430F5529

    MSP430F5529硬件spi方式驱动一个spi的液晶,可以正常显示,但是按键却无法进入中断,我的相同程序在msp430f2553中是正常的,这是什么原因造成的?

    经过排查问题,用模拟spi方式驱动就没有任何问题,我想知道根本的原因。

    void initSPI()
    {
        //SPI Pins
        P3SEL |= BIT3 + BIT4;                     // P3.3,4 option select
        P2SEL |= BIT7;
  • MSP430F5529: IAP开发问题

    Part Number: MSP430F5529
    1. 请问使用CCS V10.0的开发环境做MSP430F5529单片机的Bootload和APP的程序下可以共用同一个中断吗?我现在在Bootload和APP下使用同一个uart中断的话,一旦从Bootload程序跳转到APP的话程序就会重启,只有当我在Bootload的串口中断服务函数里面写uart中断重映射后,在APP的功能才会正常。
  • MSP430F5529: 开发板上的单片机坏了

    Part Number: MSP430F5529
    Other Parts Discussed in Thread: BQ76952EVM,

    在使用BQ76952EVM开发板调试过程中,造成TP45和3.3V短路了,现在把BQ76952EVM上的MSP430F5529取下来换块新的还能继续在开发板上开发吗,还是说要重新烧录固件

  • MSP430F5529: MSP430F5529LP 评估板使用MSP430Flasher烧录程序异常

    Part Number: MSP430F5529

    1,在windows 10上打开MSP430Flasher软件,输入任何命令行都出现闪退的情况,无法正常进行程序下载,

    2,使用MSPFlasher_1.3.20文件夹中的 .bat批处理文件,将.bat的批处理文件修改后可进行烧录操作,烧录完并读取,烧录文件与读取的文件进行对比,是一致的但是程序无法执行

  • MSP430F5529: usb和HIDI2C键盘

    Part Number: MSP430F5529

     本人画的电路图,

    HIDI2C:P3.0(UCB0SDA) 接  DN(D-)接1.5K电阻3.3V拉高,低速usb。烧写HIDI2C键盘程序。PC没有识别usb

    2:usb连接,上图虚线灰色部分丢弃,插上usb,PC也无法识别

  • MSP-EXP430F5529: MSP430F5529 USB Board Rev3.0

    Part Number: MSP-EXP430F5529

    May I ask if it is possible to provide a schematic diagram of the 3.0 version of this reference design? Not version 2.2 or 2.0, thank you very much.

    Please note that it is the schematic diagram of version 3.0!!! Not version…

  • MSP430F5529: SPI时钟(CLK)不稳定,设定的时钟周期会在一个字节中发生变化

    Part Number: MSP430F5529

    TI官网提供的关于SPI主机部分的例程,经过简单修改(仅仅修改了对应的复用端口,SIMO: P3.3, SOMI: P3.4, CLK: P2.7),在逻辑分析仪中进行测试时发现周期并不稳定,请问这是硬件自己的原因导致的吗?还是有其它方法可以进行优化改进。

  • MSP430F5529: 串口接受波特率为9600的数据并显示在OLED屏幕上读取的数据只能显示一次,会卡住不动不能一直实时显示,怀疑是串口数据量大波特率高导致串口中断溢出的问题

    Part Number: MSP430F5529

    #include <msp430.h>
    #include <driverlib.h>
    #include "system.h"
    #include "OLED.h"
    #include "MSP430F5529_I2C.h"
    #include "mpu6050.h"
    #include "uart.h"
    #include "pwm.h"…

  • MSP430F5529: CCS无法使用sprintf的%f格式化

    Part Number: MSP430F5529

    CCS中无法使用sprintf将浮点型数据转化为字符串,但是能用%d,%s就是不能用%f。我用%f时,串口打印出来的只有f

    已经将那个什么改为full,堆在上的heap也改了0x400

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    char d[100];
    float a=5.123,b=10,c=20;
    void FireWater_Test(void)
    {
    a+=10;
    b+=10;
    c+=10;
    sprintf(d,"%.2f,%.2f%.2f…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

1 2 3 4 5 »