您好,我在使用CCS内置的XDS110V2进行串口调试时,发现设备管理器的驱动识别不到了,但是之前是可以用的,请问有什么解决办法吗?

Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 12.6.0.00029)
另外我试着重新安装这里的驱动也没有解决