This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0L1306: dali_led_demo案例的使用问题

Part Number: LP-MSPM0L1306
Other Parts Discussed in Thread: MSPM0L1306

我现在使用MSPM0L1306开发板,并且试了一下MSPM0 SDK中的dali_led_demo案例。MSPM0 DALI 用户指南 — MSPM0 DALI User's Guide 1.2.0.x documentation 我有一些问题:

1.这个案例中的README文件中写着PA17引脚是UART0 TX,PA9引脚是TIMG2,请问这两个引脚是怎样连接到Mikroe DALI 2 CLICK板子上的TX和RX的?还是说不是用这两个引脚连接到Mikroe DALI 2 CLICK的?

2.我的理解是MSPM0在这个案例中是作为一个DALI从机,来接收PC软件发送到Hasseb DALI Master的相关命令。Hasseb DALI Master接线到DALI 2 CLICK转化为DALI信号,并由MSPM0接收DALI信号,然后在MSPM0执行代码中的一些方法进行调光。我的理解有问题吗?如果是这样的话,是PA0和PA1引脚和灯具连接?