Part Number: MSPM0G3507
MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x00008000
SRAM (RWX) : origin = 0x20200000, length = 0x00004000
BCR_CONFIG (R) : origin = 0x41C00000, length = 0x000000FF
BSL_CONFIG (R) : origin = 0x41C00100, length = 0x00000080
}
SECTIONS
{
.intvecs: > 0x00000000
.text : palign(8) {} > FLASH
.const : palign(8) {} > FLASH
.cinit : palign(8) {} > FLASH
.pinit : palign(8) {} > FLASH
.rodata : palign(8) {} > FLASH
.ARM.exidx : palign(8) {} > FLASH
.init_array : palign(8) {} > FLASH
.binit : palign(8) {} > FLASH
.TI.ramfunc : load = FLASH, palign(8), run=SRAM, table(BINIT)
.vtable : > SRAM
.args : > SRAM
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM (HIGH)
.BCRConfig : {} > BCR_CONFIG
.BSLConfig : {} > BSL_CONFIG
}
这是device_link.cmd文件的内存分布,根据报错信息 #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section, or the section contains padded functions. run placement with alignment fails for section ".data" size 0xeaac. Available memory ranges:。应该需要增大.data存储的空间,即SRAM,但是我在device_link.cmd文件中把length修改为0x00040000后,再次build发现文件恢复到了我修改前。请问应该如何解决呢