This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: AM2432 RGMII_RXC criteria

Part Number: AM2432


RGMII_RX manual for Tw(RXCH) 1000Mbps requirement is 3.6ns to 4.4ns, the current test time is 3.507ns~3.79ns, the minimum value does not meet the requirement;

RGMII_RX manual for Tw (RXCL) 1000Mbps requirements are 3.6ns to 4.4ns, the current test to time is 4.23ns ~ 4.458ns, the maximum value does not meet the requirements;


As above, is there any risk based on our tested out Tw(RXCH) and Tw(RXCL)1?


Please help to evaluate, thanks!

Translated with DeepL.com (free version)

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • AM2432 does not support Spread Spectrum Clocking. Tw(RXCH) and Tw(RXCL) are input parameters for AM2432 and the limits defined for this parameter were taken from the RGMII standard. It appears the attached PHY is introducing too much duty cycle distortion by creating shorter than expected high pulses and longer than expected low pulses. The AM2432 device was not validated to operate with clock pulse widths outside of the limits defined by the RGMII standard. Therefore, we expect the attached device to provide a clock that operates within the limits of 3.6ns to 4.4ns. Operating outside of the limits on a clock input could cause the RGMII receiver to do unpredictable things.