This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129DNCZAD: usb-cdc 通讯

Part Number: TM4C129DNCZAD

我现在用 TM4C129DNCZAD 这款单片机,OSC0(E19) 和 OSC1(D19) 接16MHZ 的晶振,XOSC0(T18)和XOSC1(T19) 接32768HZ的晶振,用的库是 TivaWare_C_Serial-2.2.0.295 ,PL6,PL7是USB接口。我需要实现虚拟串口的功能。
时钟配置

sc = SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ;
SysCtlClockSet(sc);
ui32SysClock = SysCtlClockFreqSet(sc,120000000);
USB引脚配置
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_USB0);
while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_USB0));
ROM_GPIOPinTypeUSBAnalog(GPIO_PORTL_BASE, GPIO_PIN_6 | GPIO_PIN_7);

windows 电脑显示是未知设备。

请问

1、上述问题可能出在哪里?
2、根据我的硬件信息,应该如何配置时钟?USB时钟该如何配置,USB引脚如何配置?
3、有没有关于TM4C129DNCZAD 的USB-虚拟串口的例程?