之前使用ST公司STM32芯片,用串口更新应用程序非常简单。
只需要改变BOOT1,BOOT0引脚的相关电平,然后使用上位机软件下载就可以实现。非常简单。
请问,TM4C如何实现用串口更新应用程序(最好列出简单的步骤,让每个工程师都能很容易实现这个功能。)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前使用ST公司STM32芯片,用串口更新应用程序非常简单。
只需要改变BOOT1,BOOT0引脚的相关电平,然后使用上位机软件下载就可以实现。非常简单。
请问,TM4C如何实现用串口更新应用程序(最好列出简单的步骤,让每个工程师都能很容易实现这个功能。)?
您好!
为了调试这个,我购买了TM4C 1294 LAUCHPAD 开发板,目前碰到现象如下:
1.先用ICDI将 C:\ti\TivaWare_C_Series-2.1.2.111\examples\boards\ek-tm4c1294xl\boot_serial下载到开发板上;使用KEIL开发环境;
2.关掉编译器,开发板重新上电;
3.使用LM FLASH PROGGRAMMER用串口下载,C:\ti\TivaWare_C_Series-2.1.2.111\examples\boards\ek-tm4c1294xl\boot_demo1,无法下载;
起始地址为0X4000,串口号选择设备管理器中的COM3,提示如下:
**ERROR* fail to establish comunication to the board! .
问题出在哪里?TI的例程是否有问题?
您好!
我参考了论坛里其他的帖子,
1.用ICDI接口将boot_serial下载到芯片,地址为0x0000,用ICDI接口将boot_demo1下载到0x4000,
2.用UART下载boot_demo2到0X4000,
之后boot_demo1和boot_demo2就可以反复下载了。
但是boot_demo1和boot_demo2下载后,程序不运行,正常应该有个LED灯在闪烁,但现在不运行,断电重新上电也不运行,不知为什么?
我用的是1294的开发板;
请各位专家回复。谢谢