Part Number: LP-AM243
hii ,
I followed the steps as TI recommendsAM243x MCU+ SDK:EVM 设置 for the UART BOOT mode and I occure a problem.

Issue Description: When executing the UART flashing process using the command:
python uart_uniflash.py -p COM12 --cfg=sbl_prebuilt/am243x-lp/default_sbl_null.cfg
The process successfully completes the first command in the configuration file (sending the flash writer):
--flash-writer=sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.hs_fs.tiimage
However, when attempting to execute the second command (flashing the application):
--file=sbl_prebuilt/am243x-lp/sbl_null.release.hs_fs.tiimage --operation=flash --flash-offset=0x0
The progress bar gets stuck at 0% and eventually fails with XMODEM protocol errors.
Environment:
- SDK: MCU+ SDK AM243x 10.01.00.32
- Board: AM243x LP
- Connection: UART via COM12, 115200 baud