尊敬的站内成员:
哪里有TM4C连接外部以太网芯片的驱动例程?
不胜感激!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
具体的驱动例程,需要看你用的什么芯片了吧,以及你芯片用的什么接口了。千兆口的话,M4的速度能达到那么高么,是不是需要上FPGA或者专门的交换机芯片呢。
谢谢您的回答哈!TM4C通过MII接口接了交换机芯片,千兆以太网芯片接在交换机芯片的其中一个port上,不知道您是否可以分享一些交换机芯片的开发经验?我是个初学者,就是自己先随便摸索
你需要说明这里TM4C的作用,他是用来干嘛的,交换机那么大的数据吞吐量,M4肯定无法胜任。
TM4C通过SPI接口配置交换机的寄存器,它通过MII接口与TM4C相连,所有的网口都通过交换机和TM4C实现网络通信。