This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C系列芯片能用seed 560 plus在ccs6.1下烧写仿真么?

Other Parts Discussed in Thread: TMS320F28377D

当前用到了两款芯片,TMS320F28377D和TM4C129X,安装的是ccs6.1开发环境,买的是SEED-560PLUS仿真器,

当然,烧写和仿真F28377D是没有任何问题的,但是用转接线连接,烧写TM4C129X就搞不定了,

想来确认一下,ccs6开发环境下,能否用seed560plus对TM4C系列芯片进行烧写仿真?

如果能,应该怎么样操作?实在是没找到相关描述文档;

如果不能(貌似也说不通,因为ccs6安装的时候是可以选择tm4c系列芯片的,如果不能用ti的仿真器烧写,在ccs下编写tm4c的程序就没有意义了!)。。。。。。

如果不能,那我就只能再去安装IAR,再去买JLINK仿真器?

实在是不想安装两种开发环境,来回切换比较麻烦。

另外,我用跳线,将seed560plus的相应3.3V、GND、TMS、TDI、TDO、TCK、TRST都连接到tm4c129x的相应引脚了,但是连接的时候说找不到时钟信号,可我确定连接的是对的啊!

求助!!!!!