Part Number: C2000WARE
Other Parts Discussed in Thread: TMDSCNCD28P55X,
I buy four piece of control card TMDSCNCD28P55X and received them today. use software : Code Composer Studio Version: 12.8.0.00012 ;
I try one Piece just now and do below step :
1, connect usb wire to usb connector J3 on control card;
2, Import a project (C:\ti\c2000\C2000Ware_5_04_00_00\driverlib\f28p55x\examples\adc\adc_ex1_soc_software) in CCS
3, when I click debug button, the CCS pop out a dialog, ask for upgrad XDS110, I click update button; upgrade finish, the software debugging is running in CCS.
4, then I try to import another project(C:\ti\c2000\C2000Ware_5_04_00_00\driverlib\f28p55x\examples\epwm\epwm_ex1_trip_zone)
5,After I building epwm_ex1_trip_zone, click debug button, CCS pop out below ERROR;
What can I do to redebugging on this control card?
thanks ,
Wangzhenning

Error initializing emulator:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
(Emulation package 12.8.0.00189)