This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,谢谢。
段时间部分芯片是不会烧毁的,理论上,上限电压是4.2V,超过了这个一段时间肯定会坏,说是上限,实际上你真4.2V工作的话,好多都可能烧坏,所以一般最好别试试。弄个LDO,或者实在不行,搞个分压电阻也是可以凑合凑合的。
MSP430F5529工作电压官方说的是1.8-3.6V
如果你非超过,好多内部的IO电路会损坏,就是整体表现还能用,实际上已经好多元件损坏了,最好别乱搞,你如果想控制5V的外设,最好通过外部驱动电路,比如三极管电路或者驱动芯片之类的。
即使是短时间,也强烈不建议您接5V供电
谢谢