This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123的systick时钟如何使用。



我想使用TM4C123的滴答时钟系统,但是发现找到的systick时钟的相关函数,但是我不知道计数值的对应关系

#if defined(TARGET_IS_TM4C123_RA1) || \
defined(TARGET_IS_TM4C123_RA3) || \
defined(TARGET_IS_TM4C123_RB1) || \
defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1)
#define ROM_SysTickValueGet \
((uint32_t (*)(void))ROM_SYSTICKTABLE[0])
#endif
#if defined(TARGET_IS_TM4C123_RA1) || \
defined(TARGET_IS_TM4C123_RA3) || \
defined(TARGET_IS_TM4C123_RB1) || \
defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1)
#define ROM_SysTickEnable \
((void (*)(void))ROM_SYSTICKTABLE[1])
#endif
#if defined(TARGET_IS_TM4C123_RA1) || \
defined(TARGET_IS_TM4C123_RA3) || \
defined(TARGET_IS_TM4C123_RB1) || \
defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1)
#define ROM_SysTickDisable \
((void (*)(void))ROM_SYSTICKTABLE[2])
#endif
#if defined(TARGET_IS_TM4C123_RA1) || \
defined(TARGET_IS_TM4C123_RA3) || \
defined(TARGET_IS_TM4C123_RB1) || \
defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1)
#define ROM_SysTickIntEnable \
((void (*)(void))ROM_SYSTICKTABLE[3])
#endif
#if defined(TARGET_IS_TM4C123_RA1) || \
defined(TARGET_IS_TM4C123_RA3) || \
defined(TARGET_IS_TM4C123_RB1) || \
defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1)
#define ROM_SysTickIntDisable \
((void (*)(void))ROM_SYSTICKTABLE[4])
#endif
#if defined(TARGET_IS_TM4C123_RA1) || \
defined(TARGET_IS_TM4C123_RA3) || \
defined(TARGET_IS_TM4C123_RB1) || \
defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1)
#define ROM_SysTickPeriodSet \
((void (*)(uint32_t ui32Period))ROM_SYSTICKTABLE[5])
#endif
#if defined(TARGET_IS_TM4C123_RA1) || \
defined(TARGET_IS_TM4C123_RA3) || \
defined(TARGET_IS_TM4C123_RB1) || \
defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1)
#define ROM_SysTickPeriodGet \
((uint32_t (*)(void))ROM_SYSTICKTABLE[6])
#endif

例如,装载值对应的是多长时间