This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

主程序.C(24): error C129: missing ';' before 'str1'



请大神帮我看看是什么问题
#include<reg52.h>
#include<intrins.h>
#include<string.h>
#include<lcd.h>
#include"hx711.h"
#include"keyboard.h"
//定义量程系数
#define idata 
#define RATIO        2144/1623
//定义标识
volatile bit FlagTest=0;     //定时测试标志位,每0.5秒置位,测完清零
volatile bit FlagKeyPress=0;     //有键按下标志,处理完毕清零
volatile bit FlagSetPrise=0;     //价格设置状态标志,设置好为1
//管脚定义
sbit LedA=P2^2;
sbit beep=P1^0;
sbit alert=P1^1;
//显示用变量
int Counter;
uchar idata str1[6]="000000";
int i,iTemp;
//称重用变量
unsigned long idata FullScale;     //满量程AD值/1000
unsigned long AdVal;     //AD采样值
unsigned long weight;     //重量值,单位g
unsigned long idata prise;     //单价,长整形值,单位为分
unsigned long idata money;     //总价,长整形值,单位为分
//键盘处理变量
uchar keycode;
uchar DotPos;      //小数点标志及位置
//整形转字符串的a函数,转换范围0--65536
void int2str(int x,car* str)
{
    int i=1;
    int tmp=10;
    while(x/tmp!=0)
    {
        i++;
        tmp*=10;
    }
 tmp=x;
 str[i]='\0';
 while(i>1)
 {
     str[--i]='0'+(tem%10);
  tmp/=10;
 }
 str[0]=tmp+'0';
}
//重新找回零点,每次测量前使用
void To_Zero()
{
    FullScale=ReadCount()/1000;
 price=0;
}
//显示单价,单位为元,四位整数,两位小数
void Display_Price()
{
    unsigned int i,j;
 display_GB2312_string(5,44,"      ");
 i=price/100;     //得到整数部分
 j=price-i*100;     //得到小数部分
 int2str(i,str1);
 
 //显示整数部分
 if(i>=1000)
 {
     display_GB2312_string(5,44,str1);
 }    
 else if(i>=100)
 {
     display_GB2312_string(5,52,str1);
 }
 else if(i>=10)
 {
     display_GB2312_string(5,60,str1);
 }
 else
 {
     display_GB2312_string(5,68,str1);
 }
 //显示小数点
 display_GB2312_string(5,76,".");
 //显示小数部分
 int2str(j,str1);
 if(j<10)
 {
     display_GB2312_string(5,84,"0");
  display_GB2312_string(5,92,str1);
 }
 else
 {
     display_GB2312_string(5,84,str1);
 }
}
//显示重量,单位kg,两位整数,三位小数
void Display_Weight()
{
    unsigned int i,j;
 display_GB2312_string(3,60,"      ");
 //weight单位是g
 i=weight/1000;     //得到整数部分
 j=weight-i*1000;     //得到小数部分
 int2str(i,str1);
 if(i>=10)
 {
     display_GB2312_string(3,60,str1);
 }
 else
 {
     display_GB2312_string(3,68,str1);    
 }
 display_GB2312_string(3,76,".");
 int2str(j,str1);
 if(j<10)
 else if(j<100)
 {
     display_GB2312_string(3,84,"0");
  display_GB2312_string(3,92,str1);
 }
 else
 {
     display_GB2312_string(3,84,str1);
 }
}
//显示总价,单位为元,四位整数,两位小数
void Display_Money()
{
     unsigned int i,j;
  display_GB2312_string(7,44,"      ");
  if(money>999999)      //超出显示量程
  {
      display_GB2312_string(7,44,"-------");
   return;
  }
  else if(i>=1000)
  {
      display_GB2312_string(7,44,str1);
  }
  else if(i>=100)
  {
      display_GB2312_string(7,52,str1);
  }
  else if(i>=10)
  {
      display_GB2312_string(7,60,str1);
  }
  else
  {
      display_GB2312_string(7,68,str1);
  }
  //显示小数点
  display_GB2312_string(7,76,".");
  //显示小数部分
  int2str(j,str1);
  if(j<10)
  {
      display_GB2312_string(7,84,"0");
   display_GB2312_string(7,92,str1);
  }
  else
  {
      display_GB2312_string(7,84,str1);
  }
}
//数据初始化
void Data_Init()
{
    price=0;
 DotPos=0;
 beep=1;
 alert=1;
}
//管脚配置
void Port_Init()
{
}
//定时器0初始化
void Timer0_Init()
{
    ET0=1;     //允许定时器0中断
 TMOD=1;     //定时器工作方式选择
 TL0=0x06;
 TH0=0xf8;     //定时器赋予初值
 TR0=1;     //启动定时器
}
//定时器0中断
void Timer0_ISR(void) interrupt 1 using 0
{
    TL0=0x06;
 TH0=0xf8;     //定时器赋予初值
 //每0.5秒钟刷新重量
 Counter++;
 if(Counter>=200)
 {
     FlagTest=1;
  Counter=0;
 }
}
 //==========main program==========//
 void main(void)
 {
     Rom_CS=1;
  initial_lcd();
  EA=0;
  Data_Init();
  Port_Init();
  Timer0_Init();
  //初始化完成,开中断
  EA=1;
  //背光
  LcdA=1;
  clear_screen();     //清除屏幕所有点
  display_GB2312_string(1,1,"电子秤初始化...");
  To_Zero();
  display_GB2312_string(1,1,"电子秤初始化成功");
  display_GB2312_string(3,1,"重量          kg");
  display_GB2312_string(5,1,"单价          元");
  display_GB2312_string(7,1,"金额          元");
  Display_Price();
  while(1)
  {
      //每0.5秒称重一次
   if(FlagTest==1)
   {
       //称重,得到重量值weight,单位为g
    AdVal=ReadCount();
    weight=FullScale-AdVal/1000;
    if(weight>0x8000)weight=0;
    weight=10000*weight/FullScale;
    weight=weight*RATIO;
    //如果超出量程,则报警
    if(weight>=10000)
    {
        beep=0;
     alert=0;
     display_GB2312_string(3,60,"------");
     display_GB2312_string(7,44,"--------");
    }
    //如果不超量程
    else
    {
        beep=1;
     alert=1;
     //显示重量值
     Display_Weight();
     //如果单价设定好了,则计算价格
     if(FlagSetPrice==1)
     {
         money=weight*price/1000;     //单位为分
      //显示总金额
      Display_Money();   
     }
     else
     {
         display_GB2312_string(7,44,"      ");
     }
     //清除测试标志
     FlagTest=0;
    }
   }
   //获取按键
   keycode=Getkeyboard();
   //有效键值0-15
   if((keyboard<16)&&(FlagKeyPress==0))
   {
       FlagKeyPress=1;
    KeyPress(keycode);
    FlagKeyPress=0;
   }
   delay(20);
  }
 }
Build target 'Target 1'
assembling STARTUP.A51...
compiling 主程序.c...
主程序.C(1): warning C500: LICENSE ERROR (R208: RENEW LICENSE ID CODE (LIC))
主程序.c(4): warning C318: can't open file 'lcd.h'
主程序.c(5): warning C318: can't open file 'hx711.h'
主程序.c(6): warning C318: can't open file 'keyboard.h'
主程序.C(24): error C129: missing ';' before 'str1'
Target not created
  • 先把第一个警告搞定,破解激活一下软件。

    前面说几个头文件都打不开,估计是因为这个。说丢失分号。看半天,没看到在哪儿丢了。看看是不是你自定义的头文件里的函数有没有丢分号的。