This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADCSequenceConfigure(,,,)函数理解



ADCSequenceConfigure(ADC0_BASE,3, ADC_TRIGGER_PROCESSOR, 0);

其中的3指的是采样序列,那它就是图片所示的PE0嘛?有什么区别啊,搞不懂

  • //*****************************************************************************
    //
    //! Configures the trigger source and priority of a sample sequence.
    //!
    //! \param ui32Base is the base address of the ADC module.
    //! \param ui32SequenceNum is the sample sequence number.
    //! \param ui32Trigger is the trigger source that initiates the sample
    //! sequence; must be one of the \b ADC_TRIGGER_* values.
    //! \param ui32Priority is the relative priority of the sample sequence with
    //! respect to the other sample sequences.
    //!
    //! This function configures the initiation criteria for a sample sequence.
    //! Valid sample sequencers range from zero to three; sequencer zero captures
    //! up to eight samples, sequencers one and two capture up to four samples,
    //! and sequencer three captures a single sample. The trigger condition and
    //! priority (with respect to other sample sequencer execution) are set.
    //!
    //! The \e ui32Trigger parameter can take on the following values:
    //!
    //! - \b ADC_TRIGGER_PROCESSOR - A trigger generated by the processor, via the
    //! ADCProcessorTrigger() function.
    //! - \b ADC_TRIGGER_COMP0 - A trigger generated by the first analog
    //! comparator; configured with ComparatorConfigure().
    //! - \b ADC_TRIGGER_COMP1 - A trigger generated by the second analog
    //! comparator; configured with ComparatorConfigure().
    //! - \b ADC_TRIGGER_COMP2 - A trigger generated by the third analog
    //! comparator; configured with ComparatorConfigure().
    //! - \b ADC_TRIGGER_EXTERNAL - A trigger generated by an input from the Port
    //! B4 pin. Note that some microcontrollers can
    //! select from any GPIO using the
    //! GPIOADCTriggerEnable() function.
    //! - \b ADC_TRIGGER_TIMER - A trigger generated by a timer; configured with
    //! TimerControlTrigger().
    //! - \b ADC_TRIGGER_PWM0 - A trigger generated by the first PWM generator;
    //! configured with PWMGenIntTrigEnable().
    //! - \b ADC_TRIGGER_PWM1 - A trigger generated by the second PWM generator;
    //! configured with PWMGenIntTrigEnable().
    //! - \b ADC_TRIGGER_PWM2 - A trigger generated by the third PWM generator;
    //! configured with PWMGenIntTrigEnable().
    //! - \b ADC_TRIGGER_PWM3 - A trigger generated by the fourth PWM generator;
    //! configured with PWMGenIntTrigEnable().
    //! - \b ADC_TRIGGER_ALWAYS - A trigger that is always asserted, causing the
    //! sample sequence to capture repeatedly (so long as
    //! there is not a higher priority source active).
    //!
    //! When \b ADC_TRIGGER_PWM0, \b ADC_TRIGGER_PWM1, \b ADC_TRIGGER_PWM2 or
    //! \b ADC_TRIGGER_PWM3 is specified, one of the following should be ORed into
    //! \e ui32Trigger to select the PWM module from which the triggers will be
    //! routed for this sequence:
    //!
    //! - \b ADC_TRIGGER_PWM_MOD0 - Selects PWM module 0 as the source of the
    //! PWM0 to PWM3 triggers for this sequence.
    //! - \b ADC_TRIGGER_PWM_MOD1 - Selects PWM module 1 as the source of the
    //! PWM0 to PWM3 triggers for this sequence.
    //!
    //! Note that not all trigger sources are available on all Tiva family
    //! members; consult the data sheet for the device in question to determine the
    //! availability of triggers.
    //!
    //! The \e ui32Priority parameter is a value between 0 and 3, where 0
    //! represents the highest priority and 3 the lowest. Note that when
    //! programming the priority among a set of sample sequences, each must have
    //! unique priority; it is up to the caller to guarantee the uniqueness of the
    //! priorities.
    //!
    //! \return None.
    //
    //*****************************************************************************

    3是系列采样的通道数,PE3这个GPIO端口号。详细见驱动库中函数说明。

  • 不一样的,采样通道,采样序列,以及ADC0/1,这是不一样的。