/********************初始化SPI********************/
void Init_SPI0(void)
{
P3SEL = 0x0E; //setup P3 for SPI mode
P3DIR |= BIT0;
UCB0CTL0 = 0x49; //Polarity,Master,8-bit, 3-Pin SPI 01001001
UCB0CTL1 = UCSSEL1 + UCSWRST; //SMCLK
UCB0BR0 = 0x82; //setup baud rate,9600
UCB0BR1 = 0x06;
UCA0CTL1 &= ~UCSWRST; //SPI EnablE
}
//******************************************************************************
// SPI_Send_OneByte,发送单个字节数据
//******************************************************************************
void SPI_Send_OneByte(uchar Send_Data)
{
P3OUT &= ~BIT0; //STE = 0
UCB0TXBUF = Send_Data; //发送一个字节
while((UCB0CTL1 & UCBUSY)==0); //等待发送完成,检测UCBUSY位
P3OUT |= BIT0; //STE = 1
}
//******************************************************************************
// SPI_Receive_OneByte,SPI接收单个字节
//******************************************************************************
uchar SPI_Receive_OneByte(void)
{
uchar ReceiveByte;
P3OUT &= ~BIT0;
UCB0TXBUF = 0xFF; //发送一个字节
while((IFG2 & UCB0RXIFG) == 0);
ReceiveByte = UCB0RXBUF;
P3OUT |= BIT0;
return ReceiveByte;
}
以上是我的SPI初始化以及传送单个字节和接受单个字节的程序。观察主控芯片的输出口的波形都是符合我要发送的数据的波形,但是主控芯片的接收口的波形是如下图一样的很奇怪的波形。每个数据端口是用3.9K电阻上拉了一个3.3V电平。没有上拉的时候波形也和图片一样。
USB118AD模块的另外一块MCU芯片msp430f149上使用就是完全正常的,主控芯片接收口的波形也是正常的高低电平。